A complete range of modern switches and accessories, designed to enrich everyday spaces with elegant design
KNOW MORERange of accessories to enrich your living environment with enhanced IoT - based user
Technology has made several advances and, in this quest, made the life of humans simpler, easier, and more comfortable
Technology has made several advances and, in this quest, made the life of humans simpler, easier, and more comfortable. The internet and mobile devices have enabled access to information anytime, anywhere. Connecting with loved ones from any place at any time has become possible. The world has become a smaller place with the advancement in technology.
Like any other industry, the electronics industry has also taken advantage of technological advances, and today, we get electrical gadgets that can be controlled using mobile devices or applications. So, the electronics industry has used technology to create remote control units that can be used to operate various electronic gadgets from anywhere, thereby adding to the comfort of the users.
Today, small electrical gadgets like fans and lights are also developed to integrate technology into them. So much so that these small devices can be operated using remote control units instead of traditional switches.
Remote control units for lights and fans can switch these gadgets on and off. For lights, the units can be used to adjust the brightness, and in the case of fans, the speed can be adjusted using these remote controls.
These remote control units are gadgets that come with a bundle of accessories. Usually, a remote control unit has a receiver unit that receives the signal of the remote controls and a remote control that is synchronised with the fan and light switches to operate them. Sometimes, the units are also provided wires to attach to the electric socket board to ensure the unit functions properly.
In addition, the remote control units are also provided with instruction manuals that can be referred to for installing, using, maintaining, and troubleshooting the remote control units.
The different types of remote control units that are available for lights and fans are wireless or wired.
The wired units connect the remote through a wire to the switchboard, and lights and fans are controlled easily. This, however, requires constant plug-in of the wires. The wired remotes are plugged into the electric socket board to operate them, and usually, the cord of these remotes needs to be long.
The wireless remote control units are the ones that operate using infrared waves to operate the fans and lights. The wireless units can also be attached to the internet to allow the comfort and ease of operating the fans and lights from anywhere and at any time. These wireless units are easier to use but must be within a specific range to use on fans and lights.
In the case of the wireless remote control units for lights, the remote control is used to operate the light regulator that is either used to brighten or dim the lights. The remotes also control the light switch to turn lights on and off. The wireless remote operates in sync with the ceiling fan regulator for fans to change the fan’s speed and turn it on and off.
Legrand Eshop offers both types of remote control units. The main advantage of using Legrand products is that they reduce energy consumption and help to manage electricity bills.
The remote control units can be installed with the help of professionals or by users alone. In either case, the instruction manual outlines the required process.
The following steps must be implemented to install a remote control unit for fans and lights.
The remotes used to operate fans and lights need to be used carefully so they do not cause trouble. Some tips for using these remotes are:
The remote control units may sometimes develop issues and fail to function properly. The users can refer to the instructions manual that provides a troubleshooting guide to fix the common problems of the remote control unit. Some of the most common problems of these remote control units are discussed below.
Remote control units for fans and lights are available in various designs, styles, and colours and can be chosen per the user’s needs. These remote control units are becoming a trend these days because of the advantages they offer.
Using remote control units for fans and lights makes operating the fans and lights easy and comfortable. With these units’ help, users can save on electricity consumption. Moreover, with advancements in technology, remote control units can also be connected to the internet and thereby controlled from anywhere, thus enabling the users to switch on and off the lights and fans as and when needed.
Legrand is one of the pioneers that develops and distributes remote control units for fans and lights at cost-effective prices. These remote control units are of the highest quality and offer users great safety. Legrand online store is the best place to buy the remote control units as it enables buyers to compare the different types of units available and purchase the ones that meet their needs.
The Legrand Eshop offers a wide range of electrical products, all of which are checked for quality and manufactured per the safety requirements and standards.
Home automation India: simplifying daily tasks with the latest technology
READ SMART SPACEGround Floor, Plot No. 603, Khata No. 457, Beside Pinak Traders, Gutuwa, Ranchi